KAS Simulator Menus Description

File Menu

Command Description
Start Start the application with the Retain Variables.
Cold Start Start the application with the initial settings
Stop Stop the application
Option Set parameters for the KAS Simulator application (see explanations below)
Exit Leave KAS Simulator application

Option

Options for Simulator

Figure 5-74: Options for KAS Simulator

Option Description
Autostart Autostart the application when KAS Simulator is launched. Autostart mode is recommended when a system is in production.

  • Parameters are saved in the Options.bin file located under:
    <user>\AppData\Local\Kollmorgen\KAS\Sinope Simulator\Resources\

Help Menu

Command Description
About Show version numbers and other Find KAS IDE Version about KAS Simulator